Vybrid VDEC questions for NTSC camera input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid VDEC questions for NTSC camera input

1,253 Views
Roshni
Contributor II

I am using the SVF5xxR with an NTSC camera (Camera output - NTSC signal with 3.58Mz color subcarrier) and have the following questions regarding the Video Decoder Module Signal Detection:

1. It is not clear in the Vybrid Reference manual, if Vybrid Video Decoder supports regular NTSC (with 3.579545 MHz color sub-carrier)? There are only references of F443 - NTSC with 4.34Mhz Chroma Subcarrier in the Reference Manual. 

2. What should be the value of VDEC_VIDMOD if auto-detection is used and the camera output's a regular NTSC signal (with 3.579545 MHz color sub-carrier)?

3. If I want to force the signal to be NTSC instead of using the auto-detection mechanism in the Video Decoder, what should be the value of MANOVR?

4. In the below snippet from the Vybrid Reference manual, its not clear why Four43_manual bit is set in the VDEC_MANOVR register for manual PAL selection. Can you please explain the same?

PAL Reference Snippet:

61.6.26 Manual Override (VDEC_MANOVR)

NOTE

Pink cast over images in PAL mode can be got rid of by writing

a value of 0xFD in this register. Upper nibble 0xF overrides

auto detect of PAL and SECAM, while lower nibble 0xD

selects PAL manually

5. The VDEC_NOISE register is 0xFF on our setup when using and NTSC camera. Are there any register settings / best practices that need to deployed to reduce the VDEC_NOISE?

Any information regarding how to use an NTSC camera with the Vybrid Video Decoder module will be greatly appreciated.

Thanks,
Roshni

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

843 Views
rendy
NXP Employee
NXP Employee