Vybrid USB in MQX 4.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid USB in MQX 4.2

Jump to solution
824 Views
kubiznak_petr
Contributor V

Why is the standard USB stack not further supported on the Vybrid platform in MQX 4.2? At least there are no project files. Instead, there are makefiles for Vybrid in the usb_v2 (even though not cloned by the cloning wizard), but no projects for IAR or DS-5. Can someone suggest a correct approach how to develop an MQX 4.2 application with USB under IAR for Vybrid?

Labels (6)
0 Kudos
1 Solution
553 Views
rendy
NXP Employee
NXP Employee

Hi,

I've just downloaded and installed MQX 4.2 and there are USB project files for Vybrid and IAR and DS5 in the new version of the stack. See attached file.

Regards
Rene Kolarik

View solution in original post

0 Kudos
2 Replies
554 Views
rendy
NXP Employee
NXP Employee

Hi,

I've just downloaded and installed MQX 4.2 and there are USB project files for Vybrid and IAR and DS5 in the new version of the stack. See attached file.

Regards
Rene Kolarik

0 Kudos
553 Views
kubiznak_petr
Contributor V

Hi Rene,

Thank you for your reply. You're right, I got confused by absence of usb_v2\build\twrvf65gs10_a5\iar directory. Apparently, the new approach is different with this stack.

0 Kudos