Hello All,
I see in the VF6xx data sheet that the PIT is supposed to be able to trigger DMA requests. However, the documentation for this seems to be lacking.
Does anyone have an example of starting a DMA transfer from a PIT without using a processor interrupt? Or is this not possible?
Thanks,
Nathan
已解决! 转到解答。
Right now, that is not possble becuase of an errata:
e4588: DMAMUX: When using PIT with "always enabled" request, DMA request does
not deassert correctly
Description:
The PIT module is not assigned as a stand-alone DMA request source in the DMA request
mux. Instead, the PIT is used as the trigger for the DMAMUX periodic trigger mode. If you want
to use one of the PIT channels for periodic DMA requests, you would use the periodic trigger
mode in conjunction with one of the "always enabled" DMA requests. However, the DMA
request does not assert correctly in this case.
Instead of sending a single DMA request every time the PIT expires, the first time the PIT
triggers a DMA transfer the "always enabled" source will not negate its request. This results in
the DMA request remaining asserted continuously after the first trigger.
Workaround:
Use of the PIT to trigger DMA channels where the major loop count is greater than one is not
recommended. For periodic triggering of DMA requests with major loop counts greater than
one, we recommended using another timer module instead of the PIT.
If using the PIT to trigger a DMA channel where the major loop count is set to one, then in
order to get the desired periodic triggering, the DMA must do the following in the interrupt
service routine for the DMA_DONE interrupt:
1. Set the DMA_TCDn_CSR[DREQ] bit and configure DMAMUX_CHCFGn[ENBL] = 0
2. Then again DMAMUX_CHCFGn[ENBL] = 1, DMASREQ=channel in your DMA DONE
interrupt service routine so that "always enabled" source could negate its request then DMA
request could be negated.
This will allow the desired periodic triggering to function as expected.
Best Regards,
Alejandro
alejandrolozano are you able to help here?