Vybrid NAK USB test mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid NAK USB test mode

256件の閲覧回数
neil3
Contributor II

I've successfully setup USB test modes on the NXP Vybrid A5 core, by following instructions in the Vybrid reference manual, section 11.1.6.3.14 (Port Test Modes -Host Operational Model).

This works for Host mode tests such as the Packet test but I cannot get the NAK (device) test to work.

What is the sequence to set up this test?

Does the device need to be set in USB Host mode or Peripheral mode?

Many thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

233件の閲覧回数
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @neil3 

 

Could you please point to me the exact document that you are referring?

 

Thank you!

 

BR,

--... ...--

Salas.

0 件の賞賛
返信

217件の閲覧回数
neil3
Contributor II

Hi @Alejandro_Salas ,

The document is "VFxxx Controller Reference Manual, F-Series, Document Number: VYBRIDRM, Rev. 8, 11/2015".

Available from here:VFxxx Controller Reference Manual - VYBRIDRM (nxp.com)

Many thanks,

Neil

0 件の賞賛
返信

200件の閲覧回数
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @neil3 

In host mode, you should see Single Ended Zero (SE0), that the both lines are pulled low. In device mode you should see NAK.

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信