Hi All-
The following document details how to get setup with a Linux virtual environment, setup the Timesys BSP/SDK, boot the board (SD card and over NFS) and shows how to debug your dual core Linux-MQX application. It was written mainly for novice Linux users, but also has plenty of detail for experienced users as well.
Any feedback is appreciated!
Thanks,
David
Hi David
This is a really nice meaty document - thanks! However...
I have followed the instructions to create a bootable Linux SD card from scratch, however I get no output at all from the serial port. I'm using the OOBE SDK from the Timesys site.
All the various steps in creating the card behave as expected (using Ubuntu under VMWare)
The demo SD that comes with the tower works fine, with exactly the same serial port setup
How do I tell if the SD card I've created is valid ?
Hi David,
Thank you for the great document !
I am having problem with DS-5 (running in Ubuntu within VirtualBox) getting hold of CMSIS-DAP. In VirtualBox, when I try to click on Devices/USB Devices/Keil Software OpenSDA CMSIS-DAP [0100], I get a "Failed to attach the USB device Keil Software openSDA CMSIS-DAP [0100] to the Virtual machine..." error.
Have you come across this problem please ?
Thanks,
Michael
 
					
				
		
When you select the OpenSDA CMSIS-DAP USB connection from VirtualBox window, give it time to install the USB drivers. This will be a windows message that says a new VirtualBox driver has been installed.
 
					
				
		
Hello
I get this error when i clicked USB devices -> Keil Software.
Already installed the Oracle_VM_VirtualBox_Extension_Pack-4.3.18-96516.
Any solution on this?