Vybrid IOMUX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid IOMUX

Jump to solution
1,093 Views
rkd
Contributor I

Hi,

is there any IOMUX tool for the vybrid series?

Could you also confirm if the following mapping is correct?

UART0:

- SCI0-TX, RX, CTS, RTS

UART1:

- SCI1-TX, RX, CTS, RTS

UART2:

- SCI2-TX, RX, CTS, RTS

UART3:

- SCI3-TX, RX, CTS, RTS


UART4:

- SCI4-TX, RX, CTS, RTS

I found all of the above on ball pin mapping.

But, 19.8.2.2 of the reference manual is telling me differently? 

Thanks

~RD

0 Kudos
Reply
1 Solution
757 Views
MehmetAliIpin
Contributor V

Dear R D,

if you dpwnload the reference manual from http://cache.freescale.com/files/32bit/doc/ref_manual/VYBRIDRM.pdf?fpsp=1&WT_TYPE=Reference%20Manual...

you will se two  excel tables on the upper left hand corner of the pdf file. These  are the IOMUX tools forr Vybrid series.

Mehmet Ali

View solution in original post

0 Kudos
Reply
1 Reply
758 Views
MehmetAliIpin
Contributor V

Dear R D,

if you dpwnload the reference manual from http://cache.freescale.com/files/32bit/doc/ref_manual/VYBRIDRM.pdf?fpsp=1&WT_TYPE=Reference%20Manual...

you will se two  excel tables on the upper left hand corner of the pdf file. These  are the IOMUX tools forr Vybrid series.

Mehmet Ali

0 Kudos
Reply