[Vybrid] Dual display, TFT + Segmented LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Vybrid] Dual display, TFT + Segmented LCD

ソリューションへジャンプ
2,247件の閲覧回数
enricpons
Contributor II

Hi all,

we have a TWR-VF65GS10 board and we would like to create our own board to test Dual Display capabilities of Vybrid, so the question is... Is it possible to have two displays at the same time ? One TFT (480x272) and one segmented (40x4). I have also a doubt. I read about de segmented controller but I don't know the way to connect (which of the pins are used).

Thank you.

Regards,

Enric

タグ(4)
1 解決策
1,947件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hi Enric,

After reviewing this, you can actually used DCU + Segment LCD. You just need to select the proper LCD for your application. Loosing LCD33 means you loose 1 front plane. For example, you can have a 38x4 LCD

Regards,

Ioseph

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,947件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Enric,

You can drive two TFT displays at the same time, no problem.

I checked the pin-out and I don't think you can drive TFT + Segmented LCD. The reason is because LCD0 to LCD43 use some of the DCU0 and DCU1 pins (TFT Display controller) I will anyway confirm this info and get back to you.

(LCD33 shares pin with DCU1_HSYNC and the rest of the LCD pins use a lot of the DCU0 signals)

Regarding the connection of LCD Segment, Vybrid, has a single Segment LCD driver with 44 LCD output signals (LCD0-LCD43) and a VLCD signal for powering the LCD

hope the info is useful.

Ioseph

0 件の賞賛
返信
1,948件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hi Enric,

After reviewing this, you can actually used DCU + Segment LCD. You just need to select the proper LCD for your application. Loosing LCD33 means you loose 1 front plane. For example, you can have a 38x4 LCD

Regards,

Ioseph

0 件の賞賛
返信
1,947件の閲覧回数
enricpons
Contributor II

Hi Ioseph,

thank you very much for your help. I will consider your comments to choose a proper LCD to have both types of displays.

Best regards and have nice vacations (in case you will enjoy comming soon (is not my case :-(  ))

Enric

0 件の賞賛
返信
1,947件の閲覧回数
enricpons
Contributor II

Hi Ioseph,

thank you for the info. I will wait until you confirm that is not possible to use at the same time TFT + Segmented LCD. Pity you can not use both types of displays just for one pin.

Also, thank you to Karina to "invoke you" :-D

Regards,

Enric