We have a custom board with a Freescale Vybrid VF610 chip and during Linux boot the system has a soft lockup.
Console dump:
...
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using ADMA
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
BUG: soft lockup - CPU#0 stuck for 23s! [swapper:1]
This only happens when the board temperature is over 47 °C.
We then observe that when the Rx signal (SCI0_RX) is grounded the system boots and everything is working fine for temperatures over 47 °C.
Any help solving this issue is highly appreciated.
Thanks For sharing this valuable information. if you like food this article is only for you guys. Wendy’s is an American multinational chain of fast-food restaurants. Wendy’s is the third-largest hamburger fast-food chain in the country. Wendy’s Breakfast Menu 2022.
Visit Here : Wendy’s Breakfast Menu 2022
Hello,
Some comments:
Regards,
Yuri.