We have a custom board with a Freescale Vybrid VF610 chip and during Linux boot the system has a soft lockup.
Console dump:
...
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using ADMA
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
BUG: soft lockup - CPU#0 stuck for 23s! [swapper:1]
This only happens when the board temperature is over 47 °C.
We then observe that when the Rx signal (SCI0_RX) is grounded the system boots and everything is working fine for temperatures over 47 °C.
Any help solving this issue is highly appreciated.
@Rikard
Hello,
NXP does not support Vybrid Linux. "The Linux BSP and support is provided by Timesys."
https://community.nxp.com/t5/Vybrid-Processors-Knowledge-Base/Vybrid-FAQ/ta-p/1103812
Regards,
Yuri.