Vybird VF610 Linux soft lockup at elevated temperatures (+ 47° C)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybird VF610 Linux soft lockup at elevated temperatures (+ 47° C)

2,984 Views
Rikard
Contributor I

We have a custom board with a Freescale Vybrid VF610 chip and during Linux boot the system has a soft lockup.

Console dump:

...

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using ADMA
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
BUG: soft lockup - CPU#0 stuck for 23s! [swapper:1]

This only happens when the board temperature is over 47 °C.

We then observe that when the Rx signal (SCI0_RX) is grounded the system boots and everything is working fine for temperatures over 47 °C.

Any help solving this issue is highly appreciated.

Labels (2)
0 Kudos
2 Replies

2,406 Views
zacharykyle
Contributor I

Thanks For sharing this valuable information. if you like food this article is only for you guys. Wendy’s is an American multinational chain of fast-food restaurants. Wendy’s is the third-largest hamburger fast-food chain in the country. Wendy’s Breakfast Menu 2022.

Visit Here : Wendy’s Breakfast Menu 2022

0 Kudos

2,973 Views
Yuri
NXP Employee
NXP Employee
0 Kudos