Vybird Cortes A5 FreeRtos Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybird Cortes A5 FreeRtos Support

723 Views
ktctuncer
Contributor I


The current eval kits come with Timesys linux for the A5 and Freescale's OS for the M4 part.

My application doesn't require Linux and I certainly like to avoid designing an external memory for the Linux. Instead I like to use  FreeRtos for the A5 and bare metal code for the M4.

Has there been a port of FreeRtos for the A5?

Labels (1)
0 Kudos
1 Reply

409 Views
FreeRTOS_org
Contributor IV

Here are a couple of pages to help - the one to follow depends on the interrupt controller used in the Vybrid:

http://www.freertos.org/Using-FreeRTOS-on-Cortex-A-Embedded-Processors.html
http://www.freertos.org/Using-FreeRTOS-on-Cortex-A-proprietary-interrupt-controller.html

There are a number of Cortex-A5 and Cortex-A9 demos (basically the same port) in the FreeRTOS download that can be used as a reference, although these are not actually running on a Vybrid so you would need to create your own project.

http://www.freertos.org/Creating-a-new-FreeRTOS-project.html