VYBrid VF6XX Cortex-M4 FPU performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VYBrid VF6XX Cortex-M4 FPU performance

Jump to solution
1,305 Views
thuanle
Contributor I

Hi everyone,

I am evaluating the VYBrid VF6XX Cortex-M4 FPU performance by using Whetstone.

However, the result of SoftVFP and FPv4-SP are same.

(I am using DS-5)

Are there any suggestion?

Thank you so much.

Best regards,

Thuan Le

Labels (1)
0 Kudos
Reply
1 Solution
883 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
4 Replies
884 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
885 Views
thuanle
Contributor I

Hi Jiri, Alejandro and all;

Thank you so much for your answer.

Sorry but... I added your code into my program and the issue still exists.

Base on the description of FPSCR: ARM Information Center

Your code will do:

- Select Alternative half-precision format.

- Any operation involving one or more NaNs returns the Default NaN.

- Flush-to-zero mode enabled.

- Select Round towards Zero (RZ) mode.

Is it correct?

This setting looks like the mode configuration for FPU, not enable the FPU.

About enable FPU in the code, I already considered about it.

I read the Cortex M4 manual, there is sample code to enable FPU for Cortex M4 as below:

; CPACR is located at address 0xE000ED88

LDR.W R0, =0xE000ED88

; Read CPACR

LDR R1, [R0]

; Set bits 20-23 to enable CP10 and CP11 coprocessors

ORR R1, R1, #(0xF << 20)

; Write back the modified value to the CPACR

STR R1, [R0]


I also check to make sure whether the FPU is really enabled or not by watching below FPU registers: FPCCR. Its value is 0xc000_0000. It means the FPU is enabled.

I also check the assembly code of my program. I can see the instruction of FPU is generated (example: VMOV.F32) and this code can run well without any exception. It also means, the FPU is already enabled.

So, I think, maybe, the enabling FPU is not the root cause of this issue.

Above is just my opinion.

Please let me know if any comment.

Thank you.

Regards,

Thuan Le

0 Kudos
Reply
885 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As Jiri mentioned, those settings need to be chagend to generate FPU instructions and to enable the FPU unit.

0 Kudos
Reply
885 Views
jiri-b36968
NXP Employee
NXP Employee

Hi Thuan,

FP have to be enabled in the compiler but also on the Vybrid - in your code.

I did that on IAR so far - item FPU

pastedImage_0.png

and wrote in your code:

#ifdef _VFPv4_

  asm ( "MOV.W r0,#0x07C00000");

  asm ( "VMSR FPSCR, r0" );

  asm ( "MOV.W r0,#0x07C00000");

  asm ( "VMSR FPSCR, r0" );

#endif

In DS-5 it should be similar:

ARM Compiler toolchain Compiler Reference: --fpu=name

Select project properties - tools setting - code generation (C/Asm)

In code use ( not sure about the macro name )

  __asm( "MOV.W r0,#0x07C00000");

  __asm( "VMSR FPSCR, r0" );

  __asm( "MOV.W r0,#0x07C00000");

  __asm( "VMSR FPSCR, r0" );

/Jiri