VF61/Vybrid, is this semaphore function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF61/Vybrid, is this semaphore function

Jump to solution
1,213 Views
soichiyamamoto
Contributor V

Hi,

I have a question about A3.4 Synchronization and semaphores(A3-12)/ DDI0406BJ_arm_architecture_reference_manual.

In the multi-core (A5+M4) of Vybrid, is this semaphore function usable?

And is exclusive control possible between multi-core(A5+M4) ?

Best Regards,

soichi yamamoto

Labels (1)
0 Kudos
Reply
1 Solution
866 Views
ed_nash
Contributor III

Hi-

Yes, there are hardware semaphores that can be (are intended to be) used between the M4 and A5.

In the case of MQX on both the A5 and M4 or Linux on the A5 and MQX on the M4, there are demos available in the Timesys BSP.

The MCC (multicore communication system) between MQX on both or Linux / MQX also uses them to protect shared memory.

One nice feature is that if access is denied, you can program the semaphore to issue an interrupt when it is freed.

I hope this helps.

Ed

View solution in original post

0 Kudos
Reply
1 Reply
867 Views
ed_nash
Contributor III

Hi-

Yes, there are hardware semaphores that can be (are intended to be) used between the M4 and A5.

In the case of MQX on both the A5 and M4 or Linux on the A5 and MQX on the M4, there are demos available in the Timesys BSP.

The MCC (multicore communication system) between MQX on both or Linux / MQX also uses them to protect shared memory.

One nice feature is that if access is denied, you can program the semaphore to issue an interrupt when it is freed.

I hope this helps.

Ed

0 Kudos
Reply