VF5xx/ FB_CS5?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VF5xx/ FB_CS5?

Jump to solution
3,604 Views
soichiyamamoto
Contributor V

Hi


Can I use FB_CS5?

FB_CSPMCR field has FB_CS5.("Vybrid Reference Manual, Rev. 5, 07/2013",P1343)

But  "Figure 8-13. FlexBus control signal multiplexing" not has FB_CS5.("Vybrid Reference Manual, Rev. 5, 07/2013",P571)


Best regards,

yamamoto

Labels (1)
1 Solution
3,180 Views
naoumgitnik
Senior Contributor V

Hello Everybody,

As per the latest information form the Design team, we do not support CS corresponding to FB_CSCR4 - only have four CSs in Vybrid.

We will have to fix the documentation.

Regards, Naoum Gitnik.


juangutierrez


View solution in original post

14 Replies
3,180 Views
juangutierrez
NXP Employee
NXP Employee

karinavalencia, can you mark Naoum reply as correct. We got confirmation from Design Team that Vybrid only have 4 FB_CS and not 5 as stated in RM. RM will be updated accordingly.

0 Kudos
Reply
3,180 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Done

3,180 Views
soichiyamamoto
Contributor V

Dear Naoum Gitnik.,

Is FB_CS5 of Flexbus an existing port in VF5xx?

Best Regards,

soichi yamamoto

0 Kudos
Reply
3,180 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

Regards, Naoum Gitnik.

3,180 Views
soichiyamamoto
Contributor V

Dear Naoum,

Thank you for reply.

Where are these(FB_CSAR5,FB_CSMR5,FB_CSCR5 for FB_CS5) registers?

A reference manual does not have mention of this register.

Best Regards,

Soichi

0 Kudos
Reply
3,180 Views
juangutierrez
NXP Employee
NXP Employee

Hi

This part of the documentation is a mess :smileysad:

There are 5 independent, user-programmable chip-select signals (FB_CS0 –FB_CS4)

However, the nomenclature used in the Multiplexing Control Register FB_CSPMCR refers the FB_CSn signals as if the counting started from 1 instead of 0 (FB_CS1 –FB_CS5). On the other hand the nomenclature for the Address, Mask and Control Registers goes from 0 to 4

So under this scheme the  mapping is

Group 1 --> FB_CS1 --> FB_CSAR0, FB_CSMR0, FB_CSCR0

Group 2 --> FB_CS4 --> FB_CSAR3, FB_CSMR3, FB_CSCR3

Group 3 --> FB_CS5 --> FB_CSAR4, FB_CSMR4, FB_CSCR4

Group 4 --> FB_CS2 --> FB_CSAR1, FB_CSMR1, FB_CSCR1

Group 5 --> FB_CS3 --> FB_CSAR2, FB_CSMR2, FB_CSCR2

0 Kudos
Reply
3,180 Views
soichiyamamoto
Contributor V

Dear Juan Antonio Gutierrez Rosas,

Thank you for reply.

> However, the nomenclature used in the Multiplexing Control Register FB_CSPMCR refers the FB_CSn signals as if the counting started from 1 instead of 0 (FB_CS1 –FB_CS5). On the other hand the nomenclature for the Address, Mask and Control Registers goes from 0 to 4

Does it mean that FB_CS0 does not exist?

If this is not the case, please give me Regster(FB_CSARx, FB_CSMRx, FB_CSCRx) of FB_CS0.

Best Regards,

soichi yamamoto

0 Kudos
Reply
3,180 Views
juangutierrez
NXP Employee
NXP Employee

It means there are only 5 FB_CSn, and there is no convention if start from 0 or from 1.

The address, mask and ctrl register for the first FB_CS will be

FB_CSAR0, FB_CSMR0, FB_CSCR0


which match the signal FB_CS MUXed by GROUP 1  (which in RM is called FB_CS1 but the correct name should be FB_CS0)

0 Kudos
Reply
3,180 Views
soichiyamamoto
Contributor V

Dear Juan Antonio Gutierrez Rosas,

Thank you for reply.

CS1, specifications of CS0 exist as follows.

Pinouts(VF6xx, VF5xx, VF3xx Data Sheet, Rev. 5, 05/2013. Freescale Semiconductor,)

PTB25→FB_CS1_b

PTB26→FB_CS0_b

Is this an error, too?

Best regards,

soichi yamamoto

0 Kudos
Reply
3,180 Views
juangutierrez
NXP Employee
NXP Employee

No, FB_CS0 does exist.

Just keep in mind there are only 5 FB_CS, Sometimes they are referred from the first one to the fifth one as FB_CS0 to FB_CS4,

but others they are referred from the first one to the fifth one as FB_CS1 to FB_CS5.

In this case

PTB26→FB_CS0_b  is the one in --> MUX Group 1  and its corresponding registers are --> FB_CSAR0, FB_CSMR0, FB_CSCR0

3,181 Views
naoumgitnik
Senior Contributor V

Hello Everybody,

As per the latest information form the Design team, we do not support CS corresponding to FB_CSCR4 - only have four CSs in Vybrid.

We will have to fix the documentation.

Regards, Naoum Gitnik.


juangutierrez


3,180 Views
naoumgitnik
Senior Contributor V

Dear Soichi,

The SW support person will check how these controls are described in our code mentioned earlier.

Regards, Naoum Gitnik.

0 Kudos
Reply
3,180 Views
karina_valencia
NXP Apps Support
NXP Apps Support

juangutierrez can you help on this case?

0 Kudos
Reply
3,180 Views
naoumgitnik
Senior Contributor V

Dear Yamamoto,

Before we proceed further, did you have a chance to look at how what you are doing in your code is handled in our SW posted on the public Vybrid web page (e.g. VF6xx Product Summary Page http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=VF6xx&fpsp=1&tab=Design_Tools_Tab, specifically the Run-time Software), please?

The reason for referring you to our code is that it is:

  • tested with our hardware and works for sure,
  • well commented and easy to understand and copy.

Regards, Naoum Gitnik.

0 Kudos
Reply