Hi This is an urgent request. I use CS5. A register cannot set only FB_CSAR4,FB_CSMR4,FB_CSCR4. ※I set a value to a register, but am readable with all 0. The debugger that I use it is DS5. A register can set the follows. FB_CSAR0 FB_CSMR0 FB_CSCR0 FB_CSAR1 FB_CSMR1 FB_CSCR1 FB_CSAR2 FB_CSMR2 FB_CSCR2 FB_CSAR3 FB_CSMR3 FB_CSCR3 Please tell me how to deal with this problem. Best Regards, soichi yamamoto
Solved! Go to Solution.
Dear Soichi,
As per the latest information form the Design team, we do not support CS corresponding to FB_CSCR4 - only have four CSs in Vybrid.
We will have to fix the documentation.
Regards, Naoum Gitnik.
Hi,
As per the chip configuration (Chapter 8 - Table 8-13. FlexBus Multiplexing) and signal multiplexing (Chapter 4 - Table 4.1 Pinouts) sections in the Vybrid reference Manual , FB_CS4_b signal is not listed for Vybrid Chip.
karinavalencia - The behaviour of writing to FB_CSAR4, FB_CSMR4, FB_CSCR4 registers is not documented in the reference manual, could you please ask one of the Freescale Applications Engineers to confirm the same.
Thanks,
Timesys Support
Hi, I get comment from you in the following thread. https://community.freescale.com/thread/312766 What is right? Be quick! We haven't much time. Best regards, soichi
Dear Soichi,
As per the latest information form the Design team, we do not support CS corresponding to FB_CSCR4 - only have four CSs in Vybrid.
We will have to fix the documentation.
Regards, Naoum Gitnik.
naoumgitnik do you have an update on this case?
Hi, I was able to obtain a reply from Local FAE. Thank you for support. soichi,
naoumgitnik can you check and confirm previous comment from Timesys?
timesyssupport can you help on this case?