VF5xx : A register cannot set only FB_CSAR4,FB_CSMR4,FB_CSCR4.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VF5xx : A register cannot set only FB_CSAR4,FB_CSMR4,FB_CSCR4.

ソリューションへジャンプ
1,892件の閲覧回数
soichiyamamoto
Contributor V

Hi This is an urgent request. I use CS5. A register cannot set only FB_CSAR4,FB_CSMR4,FB_CSCR4. ※I set a value to a register, but am readable with all 0. The debugger that I use it is DS5. A register can set the follows. FB_CSAR0 FB_CSMR0 FB_CSCR0 FB_CSAR1 FB_CSMR1 FB_CSCR1 FB_CSAR2 FB_CSMR2 FB_CSCR2 FB_CSAR3 FB_CSMR3 FB_CSCR3 Please tell me how to deal with this problem. Best Regards, soichi yamamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,623件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

As per the latest information form the Design team, we do not support CS corresponding to FB_CSCR4 - only have four CSs in Vybrid.

We will have to fix the documentation.

Regards, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,623件の閲覧回数
timesyssupport
Senior Contributor II

Hi,

As per the chip configuration (Chapter 8 - Table 8-13. FlexBus Multiplexing) and signal multiplexing (Chapter 4 - Table 4.1 Pinouts) sections in the Vybrid reference Manual , FB_CS4_b signal is not listed for Vybrid Chip.

karinavalencia - The behaviour of writing to FB_CSAR4, FB_CSMR4, FB_CSCR4 registers is not documented in the reference manual, could you please ask one of the Freescale Applications Engineers to confirm the same.

Thanks,
Timesys Support

0 件の賞賛
返信
1,623件の閲覧回数
soichiyamamoto
Contributor V

Hi, I get comment from you in the following thread. https://community.freescale.com/thread/312766 What is right? Be quick! We haven't much time. Best regards, soichi

0 件の賞賛
返信
1,624件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

As per the latest information form the Design team, we do not support CS corresponding to FB_CSCR4 - only have four CSs in Vybrid.

We will have to fix the documentation.

Regards, Naoum Gitnik.

0 件の賞賛
返信
1,623件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

naoumgitnik do you have an update on this case?

0 件の賞賛
返信
1,623件の閲覧回数
soichiyamamoto
Contributor V

Hi, I was able to obtain a reply from Local FAE. Thank you for support. soichi,

0 件の賞賛
返信
1,623件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

naoumgitnik can  you check and confirm previous comment  from Timesys?

0 件の賞賛
返信
1,623件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 件の賞賛
返信