Using QSPI1 interface on VF3XXR devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using QSPI1 interface on VF3XXR devices

1,116件の閲覧回数
martinbell
Contributor I

We are designing a board for the VF3XXR R Series Vybrid, probably the SVF311R3K1CKU2.

Our hardware engineer is planning to use QSPI1 based on the functionality listed in the Pinouts table 12.1 in the R Series Datasheet "VYBRIDRSERIESEC.pdf" - VYBRIDRSERIESEC Rev 7, 11/2014.

For example, on page 92 it lists QFP pin 47 as having ALT7 functionality of "QSPI1_A_SCK" and ditto for pins 49 to 55.

However, looking at the Device Configuration table on p.143 of the Vybrid Reference Manual, it lists the VF3XXR device as having only 1 Quad SPI.

Does this mean we can only use QSPI0 on the VF3XXR devices, even though the ALT7 functionality is listed in the pinout table for the R- Series ?

ラベル(2)
タグ(1)
0 件の賞賛
返信
0 返答(返信)