Trace on Vybrid with DS-5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trace on Vybrid with DS-5

ソリューションへジャンプ
25,825件の閲覧回数
hjk
Contributor III

I am now using TWR-VF65SG10 Tower Board , and I can boot from SD card, by the way I am on windows host

I'm trying to use DS-5 to trace on this board, and I follow the step as follow link

https://www.google.com.tw/url?sa=t&rct=j&q=&esrc=s&source=web&cd=1&cad=rja&uact=8&ved=0ahUKEwjmk7Sfs...

here's one step

"Plug in an Ethernet and connect it to your local PC. The board is set to static IP of 169.254.0.100. Set your PC to something similar like 169.254.0.1."

so I unplug my host ethernet cable, and use crossover cable to connect the target board and my host(windows)

but the ip address showed from the A5 is 192.168.1.3  so I changed the IP addr to it

"Adjust the host’s networking so that it can communicate with the target. TCP/IP (for example Ethernet) is used to communicate with the target when doing application level debug and Streamline profiling"

I change my host (win7) IP address to 192.168.1.1 and default gateway to 192.168.1.254

but it didn't work

I was wondering where did it go wrong,

ラベル(6)
1 解決策
24,087件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
23 返答(返信)
676件の閲覧回数
hjk
Contributor III

Hi timesyssupport,

What I mentioned before was Out-of-Box Demo I guessed, I haven't done any change to the SD card, I was using the original one, so I was wondering if it already have kernel gator driver and gator daemon, and if I really have to change the IP, do I have to mount the SD card to my PC and change it?

Thanks

0 件の賞賛
返信
676件の閲覧回数
kef2
Senior Contributor V

IP settings can be easily checked using ping command.

To make DS-5 Streamline happy, you need kernel gator driver and gator daemon running. Perhaps gatord isn't running and you need to start it. Both, gator kernel driver source and gator daemon sources are included in your DS-5 installation. You may need to compile them both, since your DS-5 Streamline version may require newer gator driver and daemon,than you may get form Timesys Linuxlink. See <DS-5 install dir>/arm/gator/daemon-src and .../driver-src .

0 件の賞賛
返信
676件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help to review this case?

0 件の賞賛
返信