Timesys Linux Roadmap for Vybrid 2015

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timesys Linux Roadmap for Vybrid 2015

7,336 Views
timesyssupport
Senior Contributor II

An updated Timesys Linux roadmap for Vybrid boards is available - please see the attached PDF (last updated January 25, 2015).

(minor update January 27, 2015: NFC is supported in the Jan 26th Beta release of the kernel.)

You can also view the Vybrid Release Notes for Timesys Linux, which lists current bugfixes and enhancements:

Vybrid Release Notes | Timesys Embedded Linux

For more information about the Timesys Linux 3.13 Release for Vybrid, please visit this page:

Timesys Linux 3.13 Release for Vybrid Tower Available

Thanks,

Timesys Support

12 Replies

5,662 Views
Nouchi
Senior Contributor II

Hello Timesys team,

When Kernel 3.13.x will be available ?

Emmanuel

0 Kudos
Reply

5,662 Views
timesyssupport
Senior Contributor II

Hello Emmanuel,

We are still planning for a release at the end of July.

Thanks,

Timesys Support

5,662 Views
aaronbrice
Contributor I

Timesys,

What is the status on on the updated kernel?  Is there an updated Vybrid roadmap?

Thanks,

Aaron

0 Kudos
Reply

5,662 Views
timesyssupport
Senior Contributor II

Hi Aaron,

We will release an alpha version of the 3.13 Linux kernel for the Vybrid Tower next week, along with a list of working drivers in this kernel. There will be MCC support in this kernel version, along with support for the available MCC demos as well. Let me know if you have any questions.

Thanks,

Timesys Support

0 Kudos
Reply

5,662 Views
mstuehn
Contributor I

Hi Timesys,

will the 3.13 alpha release contain all the planned features that are mentioned in the Roadmap attached to this thread?

Thanks.

0 Kudos
Reply

5,662 Views
timesyssupport
Senior Contributor II

Hi Manuel,

We have updated the roadmap with the current features in 3.13, and planned features going forward. Let me know if you have any questions.

Thanks,

Timesys Support

5,662 Views
makotokatsukura
Contributor II

Dear Timesys,

Hi Timesys.

How do I get 3.13 alpha release?

I'm really curious about the release.

Thanks,

Makoto Katsukura

0 Kudos
Reply

5,662 Views
timesyssupport
Senior Contributor II

Hello Katsukura-san,

Please visit this page for instructions for obtaining the 3.13 alpha release:

Timesys Linux 3.13 Alpha Release for Vybrid Tower Available

Thanks,

Timesys Support

0 Kudos
Reply

5,662 Views
jackblather
Senior Contributor I

Hi Timesys,

Will it have support for the Cryptographic stuff (CAAM)?

Thanks.

0 Kudos
Reply

5,662 Views
timesyssupport
Senior Contributor II

Hi Jack,

The 3.13 alpha release will not have CAAM support. We can work with you via a services agreement if this is an urgent need for you.

Thanks,

Timesys Support

0 Kudos
Reply

5,662 Views
jackblather
Senior Contributor I

Dear Timesys,

Will it still contain support for the Cryptography engine and associated modules (e.g. CAAM, CSU)?

0 Kudos
Reply

5,662 Views
timesyssupport
Senior Contributor II

Hello Jack,

Support for these modules will not be included in the July release. We don't have a schedule for these modules at this time; if this changes I will let you know.

Thanks,

Timesys Support

0 Kudos
Reply