Test SW for Vybrid CAAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Test SW for Vybrid CAAM

1,704 次查看
hari_arimilli
NXP Employee
NXP Employee

Hello,

Customer is inquiring about the availability of manufacturing test software that verifies Vybrid's Security features. Specifically, code that exercises the RNG feature of the Cryptographic Acceleration and Assurance Module (CAAM). Do we have any such software that can be provided to the customer?

Alternatively, MQX based sample code would suffice. Neither MQX nor the Linux BSP appear to support Vybrid CAAM. Are there plans for those BSPs to support CAAM?

Timesys mentions supporting CAAM but not having completed validation in this community post:

https://community.freescale.com/message/349186#349186

Can Timesys provide an update?

Thanks,

Hari

Hari Arimilli

Field Applications Engineer

Freescale Semiconductor

Cell:        612.743.1614

Email:      Hari.Arimilli@freescale.com

0 项奖励
回复
4 回复数

1,381 次查看
hari_arimilli
NXP Employee
NXP Employee

Hi Karina,

Yes, you may move it to the public community. As you have stated - the customer name and project must be removed before it is moved to the public community.

Thanks,

Hari

Hari Arimilli

Field Applications Engineer

Freescale Semiconductor

Cell: 612.743.1614

Email: Hari.Arimilli@freescale.com

0 项奖励
回复

1,381 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help to  review this case?

0 项奖励
回复

1,381 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

Timesys Support do you have an update?

0 项奖励
回复

1,381 次查看
timesyssupport
Senior Contributor II

We currently do not have software that validates CAAM with the Linux kernel. We do not currently have an estimate to when this will be available as our engineering efforts are focused on updating to an LTS kernel for Vybrid. The customer is welcome to work with us under a services agreement if this is a time-sensitive issue.

Thanks,

Timesys Support