Support GPU between X11 and wayland on I.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support GPU between X11 and wayland on I.MX6

5,087件の閲覧回数
Mihan
Contributor IV

Hi all

    I want to know the different of using GPU (opengl) between X11 and wayland on I.MX6DL.

    Because I found my Qt widget project runs with high CPU on X11, I think it doesn't use GPU to process the interface,all the paint,update are process on CPU.

    So I want to know that Wayland is better than X11 or not about GPU.

Best regards

Mihan

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

5,085件の閲覧回数
Mihan
Contributor IV

BTW, I want to paint 2D not 3D 

0 件の賞賛
返信

5,076件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello LimH,

There is no difference between Wayland and X11 in GPU the both uses it. make sure you have build it as hp your libraries or try to uses the latest yocto BSP.

 

Regards

 

0 件の賞賛
返信

5,070件の閲覧回数
Mihan
Contributor IV

Thanks @Bio_TICFSL 

   I'm building the image 4.14.98-2.0.0. for xwayland. How to know the backend it use when I compile my project?

   Can I only update the rootfs? I'm using 4.1.15-2.1.0 for X11. 

 Best regards

Mihan 

0 件の賞賛
返信