Support GPU between X11 and wayland on I.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Support GPU between X11 and wayland on I.MX6

5,191 次查看
Mihan
Contributor IV

Hi all

    I want to know the different of using GPU (opengl) between X11 and wayland on I.MX6DL.

    Because I found my Qt widget project runs with high CPU on X11, I think it doesn't use GPU to process the interface,all the paint,update are process on CPU.

    So I want to know that Wayland is better than X11 or not about GPU.

Best regards

Mihan

标签 (1)
0 项奖励
回复
3 回复数

5,189 次查看
Mihan
Contributor IV

BTW, I want to paint 2D not 3D 

0 项奖励
回复

5,180 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello LimH,

There is no difference between Wayland and X11 in GPU the both uses it. make sure you have build it as hp your libraries or try to uses the latest yocto BSP.

 

Regards

 

0 项奖励
回复

5,174 次查看
Mihan
Contributor IV

Thanks @Bio_TICFSL 

   I'm building the image 4.14.98-2.0.0. for xwayland. How to know the backend it use when I compile my project?

   Can I only update the rootfs? I'm using 4.1.15-2.1.0 for X11. 

 Best regards

Mihan 

0 项奖励
回复