Dear support,
I want to use the stop bit of UART at 2bit.
I know it is 1bit by default it.
Best regards,
Keisuke Watanabe
解決済! 解決策の投稿を見る。
Hi Keisuke,
The UART on Vybrid only supports 1 stop bit in normal usage.
However when ISO-7816 T=0 protocol is used, there is a 2-stop bits feature (see 49.4.8.2 in RM)
-Anthony
Hi,
Does it means that it is impossible to set (8,Odd,2) or (8,Even,2) on Vybrid ?
-Junichiro
Hi Keisuke,
The UART on Vybrid only supports 1 stop bit in normal usage.
However when ISO-7816 T=0 protocol is used, there is a 2-stop bits feature (see 49.4.8.2 in RM)
-Anthony
How many data bits do you need? I create 8,N,2 by 9,N,1 and abuse 9th data bit as stop bit ;-). Similar i did for 7,N,2.