SFlash configuration header

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SFlash configuration header

跳至解决方案
2,149 次查看
tfe
Contributor V

We are working on a custom vybrid-based platform, and are attempting to boot from QSPI1(Spansion S25FL256S). The image we are attempting to boot have been tested and is known to work on the TWR-VF65GS10 kit using QSPI0.

From the Vybrid Manufacturing Tool, we extracted the following header which was contained it a pre-compiled image bundled with the tool.

------------------------- SFLASH CONFIG HEADER START -------------------------

Hold delay: 0 (disabled)

Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Half Speed Delay: 0 (One clock cycle delay)

Chip Select hold time: 0

Chip Select setup time: 0

Serial Flash A1 size: 0x01000000 (16MB)

Serial Flash A2 size: 0

Serial Flash B1 size: 0x01000000 (16MB)

Serial Flash B2 size: 0

Serial Clock Frequency: 1 (60 MHz)

Mode of operation of serial Flash: 4 (Quad 4-bit data)

Serial Flash Port B selection: 0 (Port B is not used)

Dual Data Rate mode enable: 0 (DDR mode is disabled)

Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)

Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)

CS1 on Port A: 0 (Disable CS1 on Port A)

CS1 on Port B: 0 (Disable CS1 on Port B)

Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Full Speed Delay Selection: 0 (One clock cycle delay)

DDR Sampling Point: 0​

-------------------------- SFLASH CONFIG HEADER END --------------------------

We have attempted to change the "Serial Flash Port B selection" field to 1, set the size of A1 to 0x00 and B1 to 0x02000000, but unfortunately this does not work.

We have set our card to boot from fuses, and set the bootconfig appropriately. Probing the QSPI-flash chip shows that there is traffic between the MCU and chip upon boot.

Does anyone have any input?

标签 (2)
1 解答
1,873 次查看
tfe
Contributor V

I eventually figured this out myself. Only a small modification was necessary:

------------------------- SFLASH CONFIG HEADER START -------------------------

Hold delay: 0 (disabled)

Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Half Speed Delay: 0 (One clock cycle delay)

Chip Select hold time: 0

Chip Select setup time: 0

Serial Flash A1 size: 0x02000000 (32MB)

Serial Flash A2 size: 0

Serial Flash B1 size: 0

Serial Flash B2 size: 0

Serial Clock Frequency: 1 (60 MHz)

Mode of operation of serial Flash: 4 (Quad 4-bit data)

Serial Flash Port B selection: 0 (Port B is not used)

Dual Data Rate mode enable: 0 (DDR mode is disabled)

Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)

Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)

CS1 on Port A: 0 (Disable CS1 on Port A)

CS1 on Port B: 0 (Disable CS1 on Port B)

Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Full Speed Delay Selection: 0 (One clock cycle delay)

DDR Sampling Point: 0

-------------------------- SFLASH CONFIG HEADER END --------------------------

Cheers

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,874 次查看
tfe
Contributor V

I eventually figured this out myself. Only a small modification was necessary:

------------------------- SFLASH CONFIG HEADER START -------------------------

Hold delay: 0 (disabled)

Half Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Half Speed Delay: 0 (One clock cycle delay)

Chip Select hold time: 0

Chip Select setup time: 0

Serial Flash A1 size: 0x02000000 (32MB)

Serial Flash A2 size: 0

Serial Flash B1 size: 0

Serial Flash B2 size: 0

Serial Clock Frequency: 1 (60 MHz)

Mode of operation of serial Flash: 4 (Quad 4-bit data)

Serial Flash Port B selection: 0 (Port B is not used)

Dual Data Rate mode enable: 0 (DDR mode is disabled)

Data Strobe Signal enable in Serial Flash: 0 (Disable DQS)

Parallel Mode enable: 0 (Disable Parallel Mode in QSPI)

CS1 on Port A: 0 (Disable CS1 on Port A)

CS1 on Port B: 0 (Disable CS1 on Port B)

Full Speed Phase Selection: 0 (Select sampling at non-inverted clock)

Full Speed Delay Selection: 0 (One clock cycle delay)

DDR Sampling Point: 0

-------------------------- SFLASH CONFIG HEADER END --------------------------

Cheers

0 项奖励
回复
1,873 次查看
timesyssupport
Senior Contributor II

Hello,

We are currently looking into this, and attempting to determine a cause. We will follow up when we have some insight.

Thank you,

Timesys Support

1,873 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ do you have an update?

0 项奖励
回复
1,873 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ are you able  to  attend this case?

0 项奖励
回复