SDHC layout recommendations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDHC layout recommendations

Jump to solution
6,265 Views
fernandoalcaide
Contributor II

Dear,

I am designing  Board  with Vybrid VF6 and I have doubt about SDHC layout recommentaions appears in paragraph 3.3.2.3 SD Card interface requirements of ref. doc. VYBRIDHDUG_HW_UserGuide.

In this paragrap appears:

1. The clock trace should be longer than the longest trace in the Data /Command group (+5mils).

Is 5mils minimun distance or  maximum  ?

2. SD card interface layout requirements are very similar to those for the DDR one (see Section 3.5,

“DDR routing rules”).

But in this section appears DDR3 recommnedations?

I need to kown routing recomentadion to SDHC.

Can somebody help me?

Thank you in advance.

Labels (1)
1 Solution
5,997 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
5 Replies
5,998 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
5,998 Views
karina_valencia
NXP Apps Support
NXP Apps Support

jiri-b36968​ can you comment please?

0 Kudos
Reply
5,998 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Fernando,

yes, reference design uses DRAM memory type DDR3 (DDR is imprecise expression).

SDHC runs up to 50MHz.

- try to make lines short

- match all lines length.

- Add 5 mils to clk.

- try to keep lines on one layer.

- Ensure correct return path (continuous ground under lines)

- consider ESD protection if SD card is accessible to users.

/Jiri

5,998 Views
fernandoalcaide
Contributor II

Thank you

0 Kudos
Reply
5,998 Views
timesyssupport
Senior Contributor II

Hi Karina valencia Aguilar,

                                             Can the NXP Vybrid Hardware team please comment on this?

Thanks

Timesys Support

0 Kudos
Reply