Register specifications of VDEC_VIDMOD havsignal and VDEC_VSSGTH nosigthresh.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Register specifications of VDEC_VIDMOD havsignal and VDEC_VSSGTH nosigthresh.

1,522 Views
takashitakahash
Contributor III

Hi community.

Our customers have realized the NTSC camera display use the AVDC function.

Can you answer in tomorrow so we hurry the following answer.

1, About VYBRID RM of  61.6.22 Video Mode (VDEC_VIDMOD) of  havsignal.

    Please tell me the decision conditions.

    Is the level of the video signal voltage ?  or Is it the presence or absence of the synchronization signal of H sync or V sync.

2, About VYBRID RM of  61.6.27 VSync and Signal Thresholds (VDEC_VSSGTH) of  nosigthresh

    How  voltage range is the step of the decision in from bit0 bit7.

Labels (1)
0 Kudos
Reply
2 Replies

1,325 Views
richard_stulens
NXP Employee
NXP Employee

Hi Takahashi-san,

The first question is already being asked to the IP owner/IP provider.

I have asked for more information (step size) for your second question.

Is this for the same customer/project as Vybrid : VADC valid NTSC signal requirement ?

If so, can you please combine the questions in 1 thread and close this one?

Thanks & regards,

Richard

0 Kudos
Reply

1,325 Views
shigenobukatagi
NXP Employee
NXP Employee

Hi Richard, Takahashi-san,

Let's move to below thread to disscus.

https://community.freescale.com/message/573437#573437

Best Regards,

Shigenobu

0 Kudos
Reply