RESET pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,276件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I refer to the VYBRIDFSERIESEC Rev.9.

It is described as the follows at P69 NOTE.

"RESET pin has a external weak pull UP requirement if LPDDR2 memory is required to support content retention in the device low power modes where core voltage is off but DRAM voltage is on."

 

Q1.

Which is the RESET pin either T4 (RESET / RESET OUT) or D6 (DDR_RESET)?

 

Best Regards,

Eishi SHIBUSAWA

 

Dear NXP member

How about this case?

Would you please reply.

 

Best Regards,

Eishi SHIBUSAWA

ラベル(1)
0 件の賞賛
返信
1 解決策
3,020件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,021件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
3,022件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

Hello Eishi ,

It is the DDR_RESET pin that is meant here.

The pull-up is needed to prevent the pin to float when the core supplies are turned off in LPSTOP modes. IF the DDR device needs to retain the content in self-reset mode, then the pin must be pulled high  (RESET negated).

Best regards,

Richard