RESET pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RESET pin

Jump to solution
4,476 Views
eishishibusawa
Contributor III

Dear Sir

 

I refer to the VYBRIDFSERIESEC Rev.9.

It is described as the follows at P69 NOTE.

"RESET pin has a external weak pull UP requirement if LPDDR2 memory is required to support content retention in the device low power modes where core voltage is off but DRAM voltage is on."

 

Q1.

Which is the RESET pin either T4 (RESET / RESET OUT) or D6 (DDR_RESET)?

 

Best Regards,

Eishi SHIBUSAWA

 

Dear NXP member

How about this case?

Would you please reply.

 

Best Regards,

Eishi SHIBUSAWA

Labels (1)
0 Kudos
Reply
1 Solution
4,220 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
4,221 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
4,222 Views
richard_stulens
NXP Employee
NXP Employee

Hello Eishi ,

It is the DDR_RESET pin that is meant here.

The pull-up is needed to prevent the pin to float when the core supplies are turned off in LPSTOP modes. IF the DDR device needs to retain the content in self-reset mode, then the pin must be pulled high  (RESET negated).

Best regards,

Richard