Problem with VIU when using ITU656

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with VIU when using ITU656

跳至解决方案
11,984 次查看
slw
Contributor III

Hi,

We connected a analog camera to an external video-decoder (adv7180) which is connected to the viu using the 8bit itu656-interface (Vybrid VF512R3CMK4).

When we start the video-decoder it sends out the serial protocol, and we can see correctly the protocol (SAV/EAV starting with FF 00 00 XX, where XX has different state for field/vsync/hsync, ...)

The VIU detects field-irqs, but we don't get any vsync-irq.

Although we don't get any error-irqs, so it seams that the received protocol is correct (see ecc-errors in scr-register of viu), but the internal decoder from the viu-module doesn't generate a vsync-irq.

Has anybody use the viu using the 8bit itu656-mode ??

Here's the pining

PTC2 -> VIU_DATA2

PTC3 -> VIU_DATA3

PTC4 -> VIU_DATA4

PTC5 -> VIU_DATA5

PTC6 -> VIU_DATA6

PTC7 -> VIU_DATA7

PTC8 -> VIU_DATA8

PTC9 -> VIU_DATA9

PTB16 -> VIU_DATA10

PTA7 -> VIU_PIX_CLK


Another question is : How does the viu differ between 8bit and 10bit itu656-mode ?

Regards

Sebastian

标签 (2)
0 项奖励
回复
1 解答
10,913 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

we have checked all lines. If there are correctly connected to Vybrid: there is an issue on the board:

between External ADC and VIU data 2 is 10k resistor:

pastedImage_6.png

Measurement1:

Yellow is Analog

Red line is D2 (HR_VIU_DATA2) - before resitor

Green is clk

Light blue are D9 to D2

pastedImage_12.png

Red line is D2 (PTC2) - after resistor

pastedImage_13.png

So signal on D2 is not correctly connected.


Current state on terminal:

----------------------------------------------------------------------

Decoder Status (IN_LOCK):                    yes

Decoder Status (LOST_LOCK):                  no

Detected Video Standard:                      NTSC M/J

Correct line length detected:                yes

Correct field length detected:                yes

Interlaced video detected:                    yes

----------------------------------------------------------------------

Capture start !!!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

Error stopping the VIU3 device, returned: 0xffffffff

VIU3 state is ERROR, error code is 47!

Device reset !!!

VIU3 state is READY!

Capture start !!!

VIU3 state is BUSY!

VIU3 state is BUSY!

...

...


We removed R604 and placed 0R - situation has changed significantly. signal on PTC2 is correct.

After resistor removal on terminal:

----------------------------------------------------------------------

Decoder Status (IN_LOCK):                     yes

Decoder Status (LOST_LOCK):                   no

Detected Video Standard:                      NTSC M/J

Correct line length detected:                 yes

Correct field length detected:                yes

Interlaced video detected:                    yes

----------------------------------------------------------------------

Capture start !!!

VIU3 state is ERROR, error code is 7!

Device reset !!!

VIU3 state is READY!

Capture start !!!

VIU3 state is ERROR, error code is 5!

Device reset !!!

VIU3 state is READY!

Capture start !!!

VIU3 state is ERROR, error code is 5!

Device reset !!!

...

...

Error 7 is not enough lines

Error 5 is too many lines.

pastedImage_0.png

All interrupts are generated .

So now you have to change setting of the interface.

/Jiri

在原帖中查看解决方案

0 项奖励
回复
23 回复数
10,184 次查看
VilemZ
NXP Employee
NXP Employee

Hi,

I think, that you connect a few pins. If you use VIU, you need connect by VSYNC and HSYNC. Then you can use IRQ from these.

And have you got true setting of VIU? Can you send your register setting?

Regards,

Vilem

0 项奖励
回复
10,170 次查看
slw
Contributor III

Hi,

In RM (version 7) there is a table in chapter 57.3 "Video Input Signal Mapping", where HSYNC, VSYNC, DE and FID is not connected for ITU656.

In chapter 57.5.3 "Decoder" is explained that HSYNC, VSYNC and FID are extracted from the ITU656-protocol. That's why we didn't connect these signals.

Do we have to connect them ?

I have attached an register-dump in a situation where we initialized the external decoder (which sends the 656-protocol).

The field-number changes periodically, so it seems that the decoder can successfully extract it, but we don't get any VSYNC-irq.

Regards,

Sebastian

0 项奖励
回复
10,170 次查看
VilemZ
NXP Employee
NXP Employee

Hi,

It's true. I'm sorry. It is my fault. For connections:

I think that you don't need VIU_DATA10 (chapter 57.3 in RM). You need only from VIU_DATA2 to VIU_DATA9. But this connection isn't correct. VIU_DATA10 must to be connect to pin PTB19 (ALT6 for mux).

And VIU_DATA9 is not correct connection. In chapter 5.1 in RM is table for PIN MUX and for VIU_DATA9 you need connect to PTB18 (ALT6 for MUX).

Another question is : How does the viu differ between 8bit and 10bit itu656-mode ?

To avoid confusion between 8-bit and 10-bit representations, the eight most significant bits are considered to be an

integer part while the two additional bits, if present, are considered to be fractional parts

For example, the bit pattern 10010001 would be expressed as 145d or 91h, whereas the pattern 1001000101 is expressed

as 145.25d or 91.4h.

From this documet: http://www-inst.eecs.berkeley.edu/~cs150/Documents/ITU656.PDF (page 2 - NOTE 1)

Can you try now?

And why do you use external video-decoder. You can use analog input in Vybrid.

Is ok?

Vilem

0 项奖励
回复
10,170 次查看
slw
Contributor III

Hi Vilem,

I have reviewed our hardware. My connection-table above is wrong. Our hardware is connected as you described:

PTC2 -> VIU_DATA2

PTC3 -> VIU_DATA3

PTC4 -> VIU_DATA4

PTC5 -> VIU_DATA5

PTC6 -> VIU_DATA6

PTC7 -> VIU_DATA7

PTC8 -> VIU_DATA8

PTB18 -> VIU_DATA9

PTA7 -> VIU_PIX_CLK


So this is not the reason why viu doesn't work.

Does anybody use successfully the viu in itu656-mode ?


Regards

Sebastian

0 项奖励
回复
10,170 次查看
slw
Contributor III

Hi Vilem,

Any updates ?

Regards

Sebastian

0 项奖励
回复
10,170 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

I'm afraid that HSYNC_IRQ and VSYNC_IRQ interrupts as raised only when VSYNC and HSYNC signals are used (need to be confirmed with designers). ITU is using just fields (FIELD_IRQ) and VSYNC and VSYNC are decoded.

Please try to use DMA_END_IRQ (VSTART_IRQ). Do you see them raising?

/Jiri

0 项奖励
回复
10,171 次查看
slw
Contributor III

Hi Jiri,

as explained above, I only get the FIELD_IRQ. When I start the DMA-Transfer I never get an DMA_END_IRQ and DMA_ACT stays busy.

Is it even possible to use the ITU-mode without external HSYNC/VSYNC-signals connected ?

Regards

Sebastian

0 项奖励
回复
10,171 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

HSYNC/VSYNC are decoded from field in the case of ITU. No external HSYNC/VSYNC signal. Each received field triggers FIELD_INT. I would expect that is should generate also others interrupts after decoding. Since you say that it is not generated I'm going to ask designers and validation team. Stand-by.

/Jiri

10,171 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

designers claim that V/H sync should be generated in ITU mode.

Could you check if interval between FIELD_IRQ equals to one field and it is regular? Do you see correct field received - with V and H sync information?

/Jiri

0 项奖励
回复
10,171 次查看
slw
Contributor III

Hi Jiri,

Sorry for my late answer but I was ill the last 2 weeks.

I have attached some example records where you can see the relevant ITU data-stream (SAV/EAV starting 0xFF, 0x00, 0x00).

2015-01-27 13-27-32_Microsoft Excel - tek0000PAR_decoded.png

2015-01-27 13-28-19_Microsoft Excel - tek0002PAR_decoded.png

2015-01-27 13-28-34_Microsoft Excel - tek0014PAR_decoded.png

Regards

Sebastian

0 项奖励
回复
10,167 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

Thank you for data. Those data are on input of VIU interface. Do not understand their timing from those pictures, sorry. Could you correlate those data (frames) with FIELD_IRQ generation, please? In which cases it is generated and at what intervals (add toggle GPIO for example)? Or at least what is interval of FIELD_IRQ generated on your board and is it regular?

/Jiri

0 项奖励
回复
10,165 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

tested alignment on your board. Added pin output debug in VIU ISR.

So far: Field interrupt is not correctly aligned with start or end of the frame:

triggered at start of interrupt routine (peak at CH3 and 4 - trigger). Delay between start of frame and interrupt routine vary from about 300us to 6ms.

Decoding is not correct.

pastedImage_0.png

pastedImage_1.png

what is interesting it that interrupt comes always at same moment withing a line - in the middle of the line (probably latency). So we can say that it is between lines but not between correct lines:

pastedImage_0.png

ISR is alligned to HS from External ADC:

Ch4 is interrupt service routine, Ch3 is HS from external ADC

pastedImage_7.png

So wrong setting of Vybrid decoder, wrong setting of External decoder or wrong connection are valid reasons,..

pastedImage_1.png

/Jiri

0 项奖励
回复
10,914 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi Sebastian,

we have checked all lines. If there are correctly connected to Vybrid: there is an issue on the board:

between External ADC and VIU data 2 is 10k resistor:

pastedImage_6.png

Measurement1:

Yellow is Analog

Red line is D2 (HR_VIU_DATA2) - before resitor

Green is clk

Light blue are D9 to D2

pastedImage_12.png

Red line is D2 (PTC2) - after resistor

pastedImage_13.png

So signal on D2 is not correctly connected.


Current state on terminal:

----------------------------------------------------------------------

Decoder Status (IN_LOCK):                    yes

Decoder Status (LOST_LOCK):                  no

Detected Video Standard:                      NTSC M/J

Correct line length detected:                yes

Correct field length detected:                yes

Interlaced video detected:                    yes

----------------------------------------------------------------------

Capture start !!!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

VIU3 state is BUSY!

Error stopping the VIU3 device, returned: 0xffffffff

VIU3 state is ERROR, error code is 47!

Device reset !!!

VIU3 state is READY!

Capture start !!!

VIU3 state is BUSY!

VIU3 state is BUSY!

...

...


We removed R604 and placed 0R - situation has changed significantly. signal on PTC2 is correct.

After resistor removal on terminal:

----------------------------------------------------------------------

Decoder Status (IN_LOCK):                     yes

Decoder Status (LOST_LOCK):                   no

Detected Video Standard:                      NTSC M/J

Correct line length detected:                 yes

Correct field length detected:                yes

Interlaced video detected:                    yes

----------------------------------------------------------------------

Capture start !!!

VIU3 state is ERROR, error code is 7!

Device reset !!!

VIU3 state is READY!

Capture start !!!

VIU3 state is ERROR, error code is 5!

Device reset !!!

VIU3 state is READY!

Capture start !!!

VIU3 state is ERROR, error code is 5!

Device reset !!!

...

...

Error 7 is not enough lines

Error 5 is too many lines.

pastedImage_0.png

All interrupts are generated .

So now you have to change setting of the interface.

/Jiri

0 项奖励
回复
10,165 次查看
slw
Contributor III

Hi Jiri,

That's it.

We have modified our driver and now we have a live-video-stream.

Thanks for your help !

Regards

Sebastian

0 项奖励
回复
10,171 次查看
kef2
Senior Contributor V

Sebastian,

VIU interrupt flags are w1c flags. Isn't it that you clear VSYNC_IRQ while trying to clear only FIELD_IRQ?

   VIU3_SCR |= VIU3_SCR_FIELD_IRQ_MASK; // in fact clears ALL VIU3 interrupt flags.

proper way to clear only FIELD_IRQ flag would be this

   VIU3_SCR = (VIU3_SCR & ~0x003F0000) | VIU3_SCR_FIELD_IRQ_MASK;

Edward

0 项奖励
回复
10,171 次查看
slw
Contributor III

Dear Edward,

You are right. And our driver is doing it exactly this way ;-)

Problem is, that we didn't get an vsync-interrupt, even when we stop cpu using a jtag-debugger.

When cpu is in break-state we see in the viu registers that field-state toggles but there is never an vsync-irq.

Sebastian

0 项奖励
回复
10,171 次查看
naoumgitnik
Senior Contributor V

Dear Timesys Support ,

May you help the customer from the "software point view”, please?

Thanks in advance, Naoum Gitnik.

0 项奖励
回复
10,171 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help  to attend this case?

0 项奖励
回复
10,171 次查看
timesyssupport
Senior Contributor II

Hello karinavalencia and naoumgitnik,

As noted in this other thread https://community.freescale.com/thread/321908 - we do not currently have a VIU driver in the Linux kernel. There may be efforts made in the kernel update we are working on to add one, but at this time, we can offer no in depth assistance in this matter.

Regards,

Timesys Support

10,171 次查看
naoumgitnik
Senior Contributor V

Dear Sebastian,

Before we dig deeper... why are you not using Vybrid's Video ADC (VADC) inputs intended for analog video signals?

Sincerely, Naoum Gitnik.

0 项奖励
回复