Power consumption of VF6xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power consumption of VF6xx

511 Views
youngsangcho
Contributor I

Hi.

I am reviewing the spec of VF5xx and found the power consumption is about typ 400mA and max 800mA in run mode which is little higher than I expected.

Is it correct information or do you have any update ?

Labels (5)
0 Kudos
1 Reply

332 Views
naoumgitnik
Senior Contributor V

Dear Youngsang,

This in formation is correct - the max. figure reflects the temperature/voltage/process variations.

At the same time, the actual figure strongly depends on the specific application, i.e. how "heavy" the computations run by the processor are and how many of its blocks are actually used for that.

Sincerely, Naoum Gitnik.