PTB18 & PTB19

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTB18 & PTB19

Jump to solution
1,595 Views
xueweiliu
Contributor I

The latest Version of Vybrid is 1.1, I believe that the Errata for 1.0 "System: Pins PTB18 and PTB19 need to be driven at boot." has been fixed, right?

And should I need to drive these two pins when boot from RCON mode on the Vybrid 1.1 chip?

Are there some things should I pay attention to when use the two ports as GPIO or alternative function?

Thanks,

Xuewei

Tags (2)
0 Kudos
1 Solution
1,423 Views
anthony_huereca
NXP Employee
NXP Employee

Yes, there is no longer a need to drive those pins on 1.1. They can be treated like any other GPIO.

View solution in original post

0 Kudos
2 Replies
1,423 Views
xueweiliu
Contributor I

Thanks!

0 Kudos
1,424 Views
anthony_huereca
NXP Employee
NXP Employee

Yes, there is no longer a need to drive those pins on 1.1. They can be treated like any other GPIO.

0 Kudos