PHY register 32 and PHY register 33 is reverse?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PHY register 32 and PHY register 33 is reverse?

Jump to solution
896 Views
keisukewatanabe
Contributor III

Dear support,

I think that PHY register 32 and PHY register 33 is reverse.

Please see the attached file.

It can be found in the datasheet and "PHY DQ timing register for slice 2.".

However, it has been described for the DQS in Description.

"34.5.182 PHY Register 33" is the same.

My idea is correct?

Best regards,

Keisuke Watanabe

Labels (1)
0 Kudos
Reply
1 Solution
764 Views
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Yes, it is reversed: 32 is DQ. 33 is DQS. Field descriptions are indeed swaped. Thanks for letting us know, actually some one already send us the same question and we are adding a note to the manual.

Ioseph

View solution in original post

0 Kudos
Reply
1 Reply
765 Views
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Yes, it is reversed: 32 is DQ. 33 is DQS. Field descriptions are indeed swaped. Thanks for letting us know, actually some one already send us the same question and we are adding a note to the manual.

Ioseph

0 Kudos
Reply