PHY register 32 and PHY register 33 is reverse?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PHY register 32 and PHY register 33 is reverse?

跳至解决方案
878 次查看
keisukewatanabe
Contributor III

Dear support,

I think that PHY register 32 and PHY register 33 is reverse.

Please see the attached file.

It can be found in the datasheet and "PHY DQ timing register for slice 2.".

However, it has been described for the DQS in Description.

"34.5.182 PHY Register 33" is the same.

My idea is correct?

Best regards,

Keisuke Watanabe

标签 (1)
0 项奖励
回复
1 解答
746 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Yes, it is reversed: 32 is DQ. 33 is DQS. Field descriptions are indeed swaped. Thanks for letting us know, actually some one already send us the same question and we are adding a note to the manual.

Ioseph

在原帖中查看解决方案

0 项奖励
回复
1 回复
747 次查看
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Yes, it is reversed: 32 is DQ. 33 is DQS. Field descriptions are indeed swaped. Thanks for letting us know, actually some one already send us the same question and we are adding a note to the manual.

Ioseph

0 项奖励
回复