PHY register 32 and PHY register 33 is reverse?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PHY register 32 and PHY register 33 is reverse?

ソリューションへジャンプ
872件の閲覧回数
keisukewatanabe
Contributor III

Dear support,

I think that PHY register 32 and PHY register 33 is reverse.

Please see the attached file.

It can be found in the datasheet and "PHY DQ timing register for slice 2.".

However, it has been described for the DQS in Description.

"34.5.182 PHY Register 33" is the same.

My idea is correct?

Best regards,

Keisuke Watanabe

ラベル(1)
0 件の賞賛
返信
1 解決策
740件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Yes, it is reversed: 32 is DQ. 33 is DQS. Field descriptions are indeed swaped. Thanks for letting us know, actually some one already send us the same question and we are adding a note to the manual.

Ioseph

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
741件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hi,

Yes, it is reversed: 32 is DQ. 33 is DQS. Field descriptions are indeed swaped. Thanks for letting us know, actually some one already send us the same question and we are adding a note to the manual.

Ioseph

0 件の賞賛
返信