PCM052: u-boot splash screen support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCM052: u-boot splash screen support

1,559 Views
mpfgregory
Contributor III

I have managed to get the u-boot splash screen on my PMC052 working. I just wanted to share in case anybody else would like to use it.

 

You will need the 2015.04 u-boot from Toradex:

u-boot-toradex.git - U-Boot bootloader for Apalis and Colibri modules

 

The guys at Toradex have been so kind to port the DCU display driver to u-boot. You only need to add the PCM052 configuration to their u-boot. This can be done by copying the respective files from the vf610twr board. To include the display driver you can copy the respective parts from the colibri-vf board. You can find all necessary changes in the attached patch file.

 

If you are using yocto, in order to use the toradex u-boot, you need to change the meta-fsl-arm-extra/conf/machine/pcm052.conf:

--- PREFERRED_PROVIDER_u-boot = "u-boot-timesys"

+++ PREFERRED_PROVIDER_u-boot = "u-boot-toradex"

 

Then just bitbake u-boot.

 

To add a custom boot logo, add a file pcm052.bmp to git/tools/logos/ in the u-boot work directory.

 

Of course you can also add the DCU driver to the vf610twr board.

 

Best regards

 

Michael

Original Attachment has been moved to: 0001-add-pcm052-splash-screen-support.patch.zip

Labels (2)
0 Kudos
Reply
0 Replies