New Vybrid part Availability

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

New Vybrid part Availability

1,321 次查看
alansinicki
Contributor I

When will the new MVF61NS152CMK50 be available for purchase.  What exactly did NXP have to change to fix "boot" issues with the new part number and mask rev to 3N from 2N?  We are using the MVF61NS151CMK50 and the last batch of processors has extremely high current draw( over 7mA) on the RTC battery pin and are having serious boot reliability problems(1 in 10 boots fails for unknown reasons at this point).

标签 (1)
0 项奖励
回复
2 回复数

1,118 次查看
b36401
NXP Employee
NXP Employee

Here is ordering information for MVF61NS152CMK50:

https://www.nxp.com/webapp/webapp/search.partparamdetail.framework?PART_NUMBER=MVF61NS152CMK50&buyNo...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,118 次查看
ensco
Contributor I

This chip does not appear to be readily available at any of the major distributors (Digikey, Mouser, etc.) Will this change in the future or should one look at a variant?

0 项奖励
回复