New Vybrid part Availability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New Vybrid part Availability

1,323 Views
alansinicki
Contributor I

When will the new MVF61NS152CMK50 be available for purchase.  What exactly did NXP have to change to fix "boot" issues with the new part number and mask rev to 3N from 2N?  We are using the MVF61NS151CMK50 and the last batch of processors has extremely high current draw( over 7mA) on the RTC battery pin and are having serious boot reliability problems(1 in 10 boots fails for unknown reasons at this point).

Labels (1)
0 Kudos
Reply
2 Replies

1,120 Views
b36401
NXP Employee
NXP Employee

Here is ordering information for MVF61NS152CMK50:

https://www.nxp.com/webapp/webapp/search.partparamdetail.framework?PART_NUMBER=MVF61NS152CMK50&buyNo...

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,120 Views
ensco
Contributor I

This chip does not appear to be readily available at any of the major distributors (Digikey, Mouser, etc.) Will this change in the future or should one look at a variant?

0 Kudos
Reply