NOR Boot - Linux + MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NOR Boot - Linux + MQX

跳至解决方案
2,264 次查看
bfac
NXP Employee
NXP Employee

Hello!

We are evaluating the possibility of using a Flash SPI memory to boot the whole system on our product, we understand the memory size would be a limitation, but as our product will not have any display and sound we think it should fit a small NOR memory.

We think to boot the whole system from the NOR, so we should have u-boot, kernel, rootfs and mqx images on the memory, at a first analysis it looks feasible, but I wonder if this is already implemented.

The question then is:

Is the boot over SPI NOR already implemented for u-boot?

Our master core is the A5, it should boot the u-boot from NOR, and then u-boot should unpack, store and start M4 core with MQX image on internal RAM. Linux would follow regular u-boot steps to boot from DDR, rootfs should also be on DDR.

Thanks!

Bruno

标签 (4)
标记 (1)
0 项奖励
回复
1 解答
1,952 次查看
vladimirkhusain
Contributor III

Yes, this is possible to do. In fact, your configuration appears to be very close to a boot scenario descibed in Chapter 6 of this document:

http://www.emcraft.com/docs/VF6-SOM-skg-1.11.0.pdf

Boot is from a Spansion QSPI Flash device. Target platform is the Emcraft Sstems VF6 System-On-Module Starter Kit:

Vybrid VF6 SOM

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,953 次查看
vladimirkhusain
Contributor III

Yes, this is possible to do. In fact, your configuration appears to be very close to a boot scenario descibed in Chapter 6 of this document:

http://www.emcraft.com/docs/VF6-SOM-skg-1.11.0.pdf

Boot is from a Spansion QSPI Flash device. Target platform is the Emcraft Sstems VF6 System-On-Module Starter Kit:

Vybrid VF6 SOM

0 项奖励
回复
1,952 次查看
bfac
NXP Employee
NXP Employee

Thanks Vladimir!

What Linux BSP you are using? The timesys one?

0 项奖励
回复
1,952 次查看
vladimirkhusain
Contributor III

Not timesys. We (Emcraft) maintain our own BSP. It is available for free download from our web site so fell free to check the QSPI Flash boot code in U-boot.

0 项奖励
回复