NAND Flash selection for Vybrid F series MCU ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NAND Flash selection for Vybrid F series MCU ?

跳至解决方案
1,178 次查看
AhmedShameemM_H
Contributor I

Dear Sir,

We are designing freescale's Vybrid F series MCU based board, from the reference manual we understand that MCU supports for Maximum 3 address cycle NAND Flash for booting.

Can we use the NAND flash which supports 4 address cycle?

Regards,

Shameem

标签 (1)
0 项奖励
回复
1 解答
995 次查看
juangutierrez
NXP Employee
NXP Employee

My understanding is that only those commands that require up to 3 address cycles will be executed, and the rest of the commands (that require more than 3 address cycles) will be impossible to be executed

I think we should discourage the use of 4 and 5 address cycles NAND flashes for Vybrid

在原帖中查看解决方案

0 项奖励
回复
1 回复
996 次查看
juangutierrez
NXP Employee
NXP Employee

My understanding is that only those commands that require up to 3 address cycles will be executed, and the rest of the commands (that require more than 3 address cycles) will be impossible to be executed

I think we should discourage the use of 4 and 5 address cycles NAND flashes for Vybrid

0 项奖励
回复