NAND Flash selection for Vybrid F series MCU ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash selection for Vybrid F series MCU ?

Jump to solution
1,177 Views
AhmedShameemM_H
Contributor I

Dear Sir,

We are designing freescale's Vybrid F series MCU based board, from the reference manual we understand that MCU supports for Maximum 3 address cycle NAND Flash for booting.

Can we use the NAND flash which supports 4 address cycle?

Regards,

Shameem

Labels (1)
0 Kudos
Reply
1 Solution
994 Views
juangutierrez
NXP Employee
NXP Employee

My understanding is that only those commands that require up to 3 address cycles will be executed, and the rest of the commands (that require more than 3 address cycles) will be impossible to be executed

I think we should discourage the use of 4 and 5 address cycles NAND flashes for Vybrid

View solution in original post

0 Kudos
Reply
1 Reply
995 Views
juangutierrez
NXP Employee
NXP Employee

My understanding is that only those commands that require up to 3 address cycles will be executed, and the rest of the commands (that require more than 3 address cycles) will be impossible to be executed

I think we should discourage the use of 4 and 5 address cycles NAND flashes for Vybrid

0 Kudos
Reply