NAND Flash boot on Vybrid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash boot on Vybrid

1,762件の閲覧回数
Aubineau_FAE
NXP Employee
NXP Employee

Hi,

I am reading the Vybrid's manual, and I can find 2 chapters related to NAND boot:

- 19.5.6 NAND Flash Boot using NFC Interface

- 31.4.4 NAND Flash Boot

It seems that in § 31.4.4, the boot is different from §19.5.6.

Are we sure § 31.4.4 is relevant? I have the impression not...

Do have I to trust only § 19.5.6 (boot section chapter)?

Regards,

Vincent

ラベル(5)
0 件の賞賛
返信
1 返信

1,291件の閲覧回数
naoumgitnik
Senior Contributor V

Hello Vincent,

In such cases, I usually recommend to look into our software; the point is that it definitely works. Have you tried that, please?

Regards, Naoum Gitnik.

0 件の賞賛
返信