NAND Flash boot on Vybrid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND Flash boot on Vybrid

1,632 Views
Aubineau_FAE
NXP Employee
NXP Employee

Hi,

I am reading the Vybrid's manual, and I can find 2 chapters related to NAND boot:

- 19.5.6 NAND Flash Boot using NFC Interface

- 31.4.4 NAND Flash Boot

It seems that in § 31.4.4, the boot is different from §19.5.6.

Are we sure § 31.4.4 is relevant? I have the impression not...

Do have I to trust only § 19.5.6 (boot section chapter)?

Regards,

Vincent

Labels (5)
0 Kudos
Reply
1 Reply

1,161 Views
naoumgitnik
Senior Contributor V

Hello Vincent,

In such cases, I usually recommend to look into our software; the point is that it definitely works. Have you tried that, please?

Regards, Naoum Gitnik.

0 Kudos
Reply