MfgTool issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MfgTool issue

跳至解决方案
2,040 次查看
mplseng
Contributor II

When I try to use a version of u-boot built using the latest git sources, I get the error  "ModuleID[2] LevelID[1]: Failed to read HAB type from ROM!!! ".

Any suggestion as to how I can resolve this?

Bob

标签 (1)
1 解答
1,465 次查看
mplseng
Contributor II

The downloader requires a "version 3" header. The open source version of u-boot does not support this header type. We added the type which affected imximage.cfg, tools/imximage.c, and tools/imximage.h. This resolved the "HAB" error.

在原帖中查看解决方案

3 回复数
1,466 次查看
mplseng
Contributor II

The downloader requires a "version 3" header. The open source version of u-boot does not support this header type. We added the type which affected imximage.cfg, tools/imximage.c, and tools/imximage.h. This resolved the "HAB" error.

1,465 次查看
juangutierrez
NXP Employee
NXP Employee

Are you using MfgTool to flash this u-boot on SD, NAND, QSPI??

When do you see those messages, when flashing, when trying to boot?

Can you share the u-boot binary you are trying to flash to try it at my end?

0 项奖励
回复
1,463 次查看
mplseng
Contributor II

I am using the manufacturing tool to flash my build of u-boot to SD.

Attached

0 项奖励
回复