MVF61NN151CMK10/NAND flash memory and SPI flash memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MVF61NN151CMK10/NAND flash memory and SPI flash memory

895件の閲覧回数
soichiyamamoto
Contributor V

Hello

I use MVF61NN151CMK10.

NAND flash memory and SPI flash memory wants to uses  MT29F4G08ABADAWP-IT:D and M25P128-VMF6TPB.

I think that will be no problem with this method.

Is this all right?

Please give me comment.

Best Regards,

soichi yamamoto

0 件の賞賛
返信
3 返答(返信)

708件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

ioseph_martinez can you review this case and provide follow up?

0 件の賞賛
返信

708件の閲覧回数
soichiyamamoto
Contributor V

Hi Karina Valencia Aguilar,

Thank you very much.

Yes

Best Regards,

soichi yamamoto

0 件の賞賛
返信

708件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Hi Soichi-san,

I have access to the SPI NOR memory but not the NAND memory datasheet.

I checked SPI NOR memory datasheet seems fine. I expect is possible to use this device but you would need to do some testing to confirm this 100%

Regarding the NAND memory I cannot comment since I don't have access to that memory.

Which device do you plan to use for system boot, the NAND or the SPI-NOR?

Best Regards,

Ioseph

0 件の賞賛
返信