I have changed scatter file and It does not work.
I can't figure out why ?
Thank you for everything.
#! armcc -E --cpu Cortex-A5.neon
#define CODE_BASE_ADDR_START 0x3f000000
#define CODE_BASE_ADDR_END 0x3f070000
#define CODE_SIZE (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START)
#define DATA_BASE_ADDR_START 0x3f410000
#define DATA_BASE_ADDR_END 0x3f470000
#define DATA_SIZE (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)
#define DATA_SHARED_START 0x3f400000
#define DATA_SHARED_END 0x3f40fff0
#define BOOT_STACK_SIZE 0x100
#define FIQ_STACK_SIZE 0
#define ABT_STACK_SIZE 0
#define UND_STACK_SIZE 0
#define SYS_STACK_SIZE 0
LOAD_REGION_CODE CODE_BASE_ADDR_START
{
BOOT +0
{
*(STARTUP)
}
CODE +0
{
* (InRoot$$Sections) ; All library sections for example, __main.o,
; __scatter*.o, __dc*.o, and * Region$$Table
* (KERNEL)
* (TEXT)
* (+RO)
}
DATA DATA_BASE_ADDR_START ALIGN 32
{
* (+RW, +ZI)
}
; FIQ stack
FIQ_STACKS +0 ALIGN 8 EMPTY FIQ_STACK_SIZE {}
; ABT stack
ABT_STACKS +0 ALIGN 8 EMPTY ABT_STACK_SIZE {}
; UND stack
UND_STACKS +0 ALIGN 8 EMPTY UND_STACK_SIZE {}
; SYS stack
SYS_STACKS +0 ALIGN 8 EMPTY SYS_STACK_SIZE {}
KERNEL_DATA_START +0 ALIGN 16
{
* (KERNEL_DATA_START) ; start of kernel data
* (SRAM_POOL_START)
* (UNCACHED_DATA_START)
}
KERNEL_DATA_END DATA_BASE_ADDR_END - (0x03*0x10) ; RAM_END - 3 x aligned value with align 0x04
{
* (SRAM_POOL_END)
* (UNCACHED_DATA_END)
* (KERNEL_DATA_END) ; end of kernel data
}
SHARED_RAM_START DATA_SHARED_START EMPTY 0xfff0
{
}
SHARED_RAM_END DATA_SHARED_END
{
*(SHARED_RAM_END)
}
; mem_init writes a storeblock_struct at the end of kernel data,
; max size 32 bytes, so use 0x100 offset
BOOT_STACK_ADDR (DATA_BASE_ADDR_END - BOOT_STACK_SIZE) OVERLAY
{
*(BOOT_STACK)
}
; We don't use their stack or heap, but the tools expect this
; to be here, so we have a dummy placeholder.
ARM_LIB_STACKHEAP (DATA_BASE_ADDR_END - 0x100) OVERLAY EMPTY UNINIT 0x04
{
}
}