Configuring PLL1 PFD3 as the system synchronous clock at 396 MHz I have configured the CCM_CCSR(DDRC_CLK_SEL] = 1'b1 and we are getting no clock to the DRAM controller core. I am monitoring the clocks on CKO1 and CK02. I set the flags to see the ARM A5 core clock and I see the 396 MHz clock but when I switch to the DRAMC clock we get no clocks.
ARM_DIV = 1
BUG_DIV = 3
IPG_DIV = 2
PLL2 thru PLL 7 are disabled.
and
CCGR6 = 0xFFFFFFFF
Not sure what I am missing to enable this.
*******************************************************************************************************************
*
*
* Solution has been found it seems to be a bug in the silicon. Could somebody at Freescale verify this.
*
*
*******************************************************************************************************************
For the DRAMC clock GL MUX to work properly both the PLL2 PFD2 Clock and SYS_DIV_OUT_CLK must
be active when the CCM_CCSR[DDRC_CLK_SEL] bit is set to configure it from its default of
[PLL PFD2 selection] 1'b0. By having the PLL PFD2 clock running the DRAMC clock output can switch to
the SYS_DIV_OUT_CLK. Following is the code we used to configure the clock tree in our system and it
works around this issue.
/*******************************************************
* Setup the clocks to run in synchronous mode
* using PLL1 PFD3. The rest of the system uses PLL1 PFD 4
* at the same frequency
*/
/* CCM_CCGR1
WDOG-M4, WDOG-A5, TCON0, RSVD, ADC0, RSVD, FTM1, FTM0, PIT, PDB, RSVD, USBC0, CRC, SAI3, SAI2, SIA1
00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 11, 00, 00, 00, 00
*/
CCM->CCGR1 = 0x00000300;
/* CCM_CCGR2
RSVD, RSVD, PORT E MUX, PORT D MUX, PORT C MUX, PORT B MUX, PORT A MUX, IOMUX, RSVD, RSVD, RSVD, QUADSPI0, RSVD, RLE, RSVD, LPTMR
00, 00, 11, 11, 11, 11, 11, 11, 00, 00, 00, 00, 00, 00, 00, 00
*/
CCM->CCGR2 = 0x0FFF0000;
/* CCM_CCGR3
RSVD, RSVD, RSVD, RSVD, RSVD, RSVD, RSVD, DCU0, RSVD, RSVD, RSVD, RSVD, RSVD, SCSCM, RSVD, ANADIG
00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 01, 00, 01
*/
CCM->CCGR3 = 0x00000011;
/* CCM_CCGR4
ASRC, SPDIF, ESAI, RSVD, RSVD, EWM, I2C 0, I2C 1, RSVD, RSVD, WKUP, CCM, GPC, VREG_DIG, RSVD, CMU
00, 01, 00, 01, 01, 01, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00
*/
CCM->CCGR4 = 0x11500000;
/* CCM_CCGR5 --> reserved */
/* CCM_CCGR6
RSVD, DDRMC, SPI3, SPI2, RSVD, UART5, UART4, WDOG_SNVS, SNVS, RSVD, OTP_CTRL, RSVD, RSVD, DMA3, DMA2, RSVD
00, 11, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00
*/
CCM->CCGR6 = 0x30000000;
/* CCM_CCGR7
RSVD, LCD, TCON1, RSVD, ADC1, RSVD, FTM3, FTM2, RSVD, RSVD, RSVD, USBC1, RSVD, SDHC1, SDHC0, RSVD -->
00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 00, 11, 00, 11, 11, 00 -->
*/
CCM->CCGR7 = 0x0000033C;
/* CCM_CCGR8 thru CCM_CRGR11
No modules used in these register
*/
CCM->CCGR8 = 0x0; //Turn off GPU since causes immediate interrupt
CCM->CCGR9 = 0x0;
CCM->CCGR10 = 0x0;
CCM->CCGR11 = 0x0;
/* enable the external oscillator */
/* CCM_CLPCR
Clear FXOSC_PWRDWN bit before enabling external fast oscillator.
*/
CCM->CLPCR = 0x00000078;
/* CCM_CCR
Enable external fast oscillator.
*/
CCM->CCR = 0x00011000;
/* ANADIG_ANA_MISC0
Clear ANA_MISC0[CLK_24M_IRC_XTAL_SEL] to select among external and internal fast oscillator.
*/
ANADIG->ANA_MISC0 = 0x00000000;
/* Enable and configure PLLs */
/* PLL 1
[18] PFD_OFFSET_EN = 1'b0
[17]DITHER_ENABLE = 1'b0
[16]BYPASS = 1'b0
[14]BYPASS_CLK_SRC = 1'b0
[13]ENABLE = 1'b1
[12]POWER_DOWN = 1'b0
[0] DIV_SELECT = 1'b1
*/
ANADIG->PLL1_CTRL = 0x00002001;
ANADIG->PLL1_PFD = 0x18181593;
/* PLL 2 PFD2 is only configured due to an issue with the DRAMC clock mux.
These are disabled after the clocks are set up
*/
ANADIG->PLL2_CTRL = 0x00002001;
ANADIG->PLL2_PFD = 0x98981898;
/* Configure MUX selectors for core, bus and peripheral clocks.
CCM_CCSR:
[31] PLL3_PFD4_EN = 1'b0
[30] PLL3_PFD3_EN = 1'b0
[29] PLL3_PFD2_EN = 1'b0
[28] PLL3_PFD1_EN = 1'b0
[24] DAP_EN= 1'b0
[21:19] PLL2_PFD_CLK_SEL = 3'b000 -> PLL2 main clock
[18-16] PLL1_PFD_CLK_SEL = 3'b011 -> PLL1 PFD3 clock
[15] PLL2_PFD4_EN = 1'b0
[14] PLL2_PFD3_EN = 1'b0
[13] PLL2_PFD2_EN = 1'b0
[12] PLL2_PFD1_EN = 1'b0
[11] PLL1_PFD4_EN = 1'b1
[10] PLL1_PFD3_EN = 1'b1
[ 9] PLL1_PFD2_EN = 1'b1
[ 8] PLL1_PFD1_EN = 1'b0
[ 6] DDRC_CLK_SEL = 1'b1 -> SYS_DIV_OUT_CLK
[ 5] FAST_CLK_SEL = 1'b1 -> FX0SC clock
[ 4] SLOW_CLK_SEL = 1'b0 -> IRC clock
[2:0] SYS_CLK_SEL = 3'b100 -> PLL1_PFD_CLK_SEL
*/
/* Issue cannot use 0x00030E64 directly because the DDRC_CLK_SEL mux will
not switch to right clock source without PLL2 PFD2 Clock
*/
CCM->CCSR = 0x00032E64;
/* Configure clock dividers for core, bus and peripheral clocks.
CCM_CACRR:
[24:22] FLEX_CLK_DIV = 3'b000
[21] PLL6_CLK_DIV = 1'b0
[20] PLL3_CLK_DIV = 1'b0
[17:16] PLL1_PFD_CLK_DIV = 2'b00
[12:11] IPG_CLK_DIV = 2'b01
[8:6] PLL4_CLK_DIV = 3'b000
[5:3] BUS_CLK_DIV = 3'b010
[2:0] ARM_CLK_DIV = 3'b000
28 24 20 16 12 8 4 0
0000_0000_0000_0000_0000_1000_0001_0000
*/
CCM->CACRR = 0x00000810;
/* PLL 3 -> Disabled at start up is enabled by software
when the USB port is connected. USB is the only
device that uses this PLL.
*/
ANADIG->PLL3_CTRL = 0x00001001;
/* PLL 4 -> disabled */
ANADIG->PLL4_CTRL = 0x00001001;
/* PLL 5 -> disabled */
ANADIG->PLL5_CTRL = 0x00001001;
/* PLL 6 -> disabled */
ANADIG->PLL6_CTRL = 0x00001001;
/* PLL 7 -> disabled */
ANADIG->PLL7_CTRL = 0x00001001;
/* Disable PLL2 now that the DRAMC clock mux has been configured
*/
ANADIG->PLL2_CTRL = 0x00001001;
CCM->CCSR = 0x00030E64;