Hi all,
I'm encountering a very strange issue with the L2_swtich on Vybrid, using linux 3.0, and i've the same problem on our custom board, phytec board and freescale twr board.
All my board are in static IP.
My PC is connected to the ETH0 port on board. I connect the ETH1 on a switch in my local network. This switch is connected to a router for internet access.
From my pc, i can ping all members in the local network and i can access to internet.
Here is the problem : I can't acces website ( on other things like ssh or ftp connection) in my LOCAL network.
I've a full acces on WAN, i can ping all member in LAN, but it seems like if the data's are too big (or too much datas) from the local network, the switch don't work.
I've tried with only 2 board and 1 pc connected : The pc on ETH0 and the second board on ETH1, all with static IP. I'm able to ping both board. I can access the first board embedded website, but i can't access the second...
It's like if there is a big set of data in short time, I lost the frames. Does the switch is fast enought?
I've also tried to reduce data speed to 10T (i was using Auto Negociation) but it d'ont change anything.
Any idea?
 
					
				
		
Hello,
It's been a long time however I cannot manage it this to work without dual FEC and software bridge. Did you find any fix ? Do you know if @timesyssupport applied any fix in the past ?
Thank you in advance,
 
					
				
		
Hello,
I'm also facing a similar problem using L2 switch. Whenever I have a peak of data runing through I loose packages.
Did manage to fix it ? Do you have any update from timesys ?
Thank you in advance,
Hello,
I was using the linux 3.0.15 from Timesys. I know they release new version since I was using it but I don't know if they fix it.
On our custom board, I've disable the support for L2_SWITCH and I'm using the dual FEC with BRIDGE. It make a software switch
 
					
				
		
Thank you for your prompt reply.
I wanted to avoid the software switch, however I'll give it a try.
 
					
				
		
Hello Jemery,
We are investigating this issue, as Phytec has inquired about this as well. Once we have had a chance to reproduce and analyze, we will follow up.
Thank you,
Timesys Support
Hello,
Thank you, i'm waiting for your answer.
regards.
Have you some news ?
Were you able to reproduce this issue?
 
					
				
		
Hello Jeremy,
Could you share your kernel config for this issue?
In this case, CONFIG_FSL_L2_SWITCH and CONFIG_FEC cannot be enabled at the same time, only one or the other.
How are you confirming that frames are lost? If you can provide an exact procedure we can attempt to reproduce.
If you have not already, please submit a support request in the Timesys Support queue - that is accessible by logging into: http://linuxlink.timesys.com and clicking the "Support" link.
Thank you,
Timesys Support
Hello,
Here is my .config file
It's the default .config from factory
I've made a new "factory" folder, using twr_vf600-factory-installer.sh, and i used the default .config file. I remove the FEC and enable L2_Switch, and because i'm using the freescale tower_board with a twr_ser2 card, I change the PHY driver to the good one : Drivers for National Semiconductor dp83848 dp83849 PHYs
My /network/interfaces file is :
auto eth0
iface eth0 inet static
address 192.168.3.42
network 192.168.3.0
netmask 255.255.255.0
broadcast 192.168.3.255
gateway 192.168.3.25
With this config, i simply plug an ethernet cable from my pc to the TWR, and a second cable from the TWR to a 30 slot ethernet switch on my local network.
Now for test :
- ping is OK. I can ping local devices or ping www.google.fr, it works fine.
- web access : I can access website through my router. (like www.google.com, www.youtube.com ...) it works.
- Local web access : It not work! I can't load the website of my printer for example. on wireshark i can see that the first packet is received, but not the nexts.
- ssh on local device : i can't access to my local device in SSH.
- ftp : It's weir, i can acces device when there is not a lot of repertories to load. I can't if there is a lot of repertories. It's like if there is a lot of repertories to load, I lost frames and the connection is lost.
I will submit a support request on timesys website.
EDIT : I add some screenshot.
The first , "page_good.png" is the page i must load from my device (ip addr 192.168.3.62, in my LOCAL network). This device is connected to my local network, I load this page when i was NOT connected to the TWR_BOARD switch.
The second, "page_bug_switch.png", show you what I get when I try to connect to my embedded website USING the TWR_BOARD switch. My pc is connected to the freescale TWR_Board and the TWR is connted to the device. The webpage is loading continusly but i don't get it.
The "wireshark_switch_bug.png" is the wireshark capture when i'm trying to get the website through the TWR_Board switch. You can see that the TCP connection is well done. I get the first packet but after there is a problem.
Looking wireshark, i've noticed that a big amount of data in a short time don't pass through the switch.I
I don't know if it's the driver or if it's a hardware issue, but i only get this issue with the switch. And i was able to reproduce this bug using phytec board, freescale board, and with the default .config file, i simply change the FEC for L2_SWITCH in kernel.
workaround :
If someone is having this bug and need switch ability, I'm using a trick: enable "Bridge" and the "dual fec" in kernel and use "bridge-utils" software, you get a software switch. .
 
					
				
		
 karina_valencia
		
			karina_valencia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		timesyssupport please continue with the follow up.
 
					
				
		
Hello karinavalencia and jeremyesquirol,
Thank you for providing this additional information; we will provide this to our Vybrid engineers for further review and follow up.
Thank you,
Timesys Support
 
					
				
		
 karina_valencia
		
			karina_valencia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Timesys Support do you have an update?
 
					
				
		
 karina_valencia
		
			karina_valencia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		timesyssupport do you have an update?
 
					
				
		
 karina_valencia
		
			karina_valencia
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		timesyssupport do you have an update or can let us know an estimated due date?
 
					
				
		
Hello,
I'm still facing same problem and could not find an answer anywhere. Has been any fix released ? Is there a way to fix it that other than using dual FEC and software switching ?
Thank you in advance,
Hi
It seems that ESW seems working or not working depending on network infrastructure. Connecting way [A] everything seems being fine. Ping to local network behind Cisco IP phone, access to network resources on local network and internet:
PC <-> [TWRSER2 with ESW switch] <-> <Cisco IP phone with two port switch> <--> network
Connecting way [B] only ping works to everywhere, no problems pinging various www hosts on local network and internet. But it is impossible to display any www pages from local network and internet:
PC <-> [TWRSER2 with ESW switch] <-> [home network with TP-Link router]
It seems the missing part is ESW_MODE.CRCTRAN=1. Driver keeps this bit cleared. Setting this bit from JTAG debugger makes everything working well in connection variant B. Did retest connection variant A, but I guess it should be fine as well.
See switch_enet_init() and switch_restart() routines.
Try replacing
writel(FSL_ESW_MODE_SW_EN, fep->membase + FEC_ESW_MODE);
with
writel(FSL_ESW_MODE_SW_EN | FSL_ESW_MODE_CRC_TRAN, fep->membase + FEC_ESW_MODE);
Edward