Is there a DCU4 driver on the M4 core for MQX?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a DCU4 driver on the M4 core for MQX?

ソリューションへジャンプ
1,605件の閲覧回数
markwatson
Contributor III

I have noted the presence of a driver for the DCU4 in the A5 BSP, but not in the M4 BSP.  Is there a driver and/or example code for running the DCU from the M4 core?  Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,469件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,470件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,470件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I think the only concern is that MQX for the M4 only executes out of iRAM and to handle pictures you need the DDR which is configured only for the CA5 target.

/Alejandro

0 件の賞賛
返信
1,470件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi, no there isn't such an example, but the DCU driver should work on both cores. You should be able to port the A5 example to M4 core smoothly.

Regards

Rene