Inter-core IRQ collisions on Vybrid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Inter-core IRQ collisions on Vybrid

ソリューションへジャンプ
1,531件の閲覧回数
kubiznak_petr
Contributor V

Having two GPIO inputs on the same PORT (say PTB23 and PTD10, both being on PORT2), how do I properly configure the interrupts, so that one GPIO triggers the ISR on A5 only and the second on M4 only?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
1,326件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Petr,

sorry for delay. In this  case only main core is capable of manage interrupts.

Regards,

Carlos

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,327件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Petr,

sorry for delay. In this  case only main core is capable of manage interrupts.

Regards,

Carlos

0 件の賞賛
返信