Inter-core IRQ collisions on Vybrid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inter-core IRQ collisions on Vybrid

Jump to solution
1,713 Views
kubiznak_petr
Contributor V

Having two GPIO inputs on the same PORT (say PTB23 and PTD10, both being on PORT2), how do I properly configure the interrupts, so that one GPIO triggers the ISR on A5 only and the second on M4 only?

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
1,508 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Petr,

sorry for delay. In this  case only main core is capable of manage interrupts.

Regards,

Carlos

View solution in original post

0 Kudos
Reply
1 Reply
1,509 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Petr,

sorry for delay. In this  case only main core is capable of manage interrupts.

Regards,

Carlos

0 Kudos
Reply